CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimEngineeringUnits Json Schema
CimEngineeringUnits Json Schema
Description
object contains the conversion information for converting a point from raw device units to real-world units. Conversion can either be linear or based on a conversion expression
Overview
CimEngineeringUnits
object contains the conversion information for converting a point from raw device units to real-world units. Conversion can either be linear or based on a conversion expression
EuExpression : string
is a string containing the equation used to convert the value from device units to engineering units. To use a custom expression you must first disable the linear conversion for the object. If the point is not read-only a reverse expression must be specified to allow a setpoint in engineering units to be translated back to device units. It is your responsibility to make sure these expressions yield the correct results
EuLabel : string
is a string containing the EuLabel. Note you cannot specify an EuLabel if using a measurement unit for the point
EuRevExp : string
is a string containing the equation used to convert the value from engineering units to device units. To use a custom expression you must first disable the linear conversion for the object. A forward expression must also be specified. It is your responsibility to make sure these expressions yield the correct results
HighConvValue : string
is a variant containing the high converted value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to True
HighRawValue : string
is a variant containing the upper raw value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to True
LinearConversion : boolean
is a boolean indicating if the conversion is linear or custom
LowConvValue : string
is a variant containing the low converted value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to True.
LowRawValue : string
is a variant containing the low raw value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to True.
Properties
NameDescriptionData Type
is a string containing the equation used to convert the value from device units to engineering units. To use a custom expression you must first disable the linear conversion for the object. If the point is not read-only a reverse expression must be specified to allow a setpoint in engineering units to be translated back to device units. It is your responsibility to make sure these expressions yield the correct resultsstring
is a string containing the EuLabel. Note you cannot specify an EuLabel if using a measurement unit for the pointstring
is a string containing the equation used to convert the value from engineering units to device units. To use a custom expression you must first disable the linear conversion for the object. A forward expression must also be specified. It is your responsibility to make sure these expressions yield the correct resultsstring
is a variant containing the high converted value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to Truestring
is a variant containing the upper raw value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to Truestring
is a boolean indicating if the conversion is linear or customboolean
is a variant containing the low converted value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to True.string
is a variant containing the low raw value used for linear conversion with a string representation of 10 characters or less. Larger values will be rejected. To use linear conversion you must set linear conversion to True.string
See Also